Part Number: TPS2052B Dear Specialists,
My customer needs IEC62368-1:2018(3rd) CB Certified Report.
Could you please provide it?
In the product folder I could find IEC62368-1:2014(2nd) version, however I could not find IEC62368-1:2018(3rd) version.
If it…
Part Number: TPS2052B Hi,
Please kindly review below silk-screen, and our customer consider the second line is different, and the IQC deperatment has some query, thanks.
Part Number: TPS2052B Hello,
I want to know if the temparature range for TPS2052BDRBT and TPS2052BDRBR are correct on the datasheet.
To my knowledge, the last digit in the part number's nomenclature represents the packing options between a 3000 and 250…
Part Number: TPS2052B Other Parts Discussed in Thread: TPS2051 , TPS2061 Hi Team,
My customer will use our TPS2052B. What is the CC current when OCP triggered. The waveform and parameter in datasheet are not match.
Best regards,
Hardy
Hi Bob, Good day. I've got a response from our customer, kindly see below. thank you for the feedback. I was doing some measurements with TPS2052B. Voltage of 5 V was present at IN pin and 0 V at EN pin (switch diasbled). There was only capacitive…
Part Number: TPS2052B Hello guys,
One of my customes is considering using TPS2052B for their new products.
They need a equivalent schematic of termianals of EN1, EN2, OC1, OC2 of TPS2052B
for their failure analysis.
Could you give me the equivarent schematic…
Part Number: TPS2052B Other Parts Discussed in Thread: TPS2052 Hi,
I have given enough power to My USB hub usb2514B so that en1 to en4 is logic high and tps2052B got active so that I can get vout1 to vout4 5V, 500 mA.
I have used 2 tps2052b but when I…
Part Number: TPS2052B Hi Team,
Does TPS2052B will plan to EOL? or still in supply ?
due to customer heard that TI not recommend to use TPS2052B for new project now.
thanks,
Mark
Part Number: TPS2052B Dear TI,
Could you please tell me what different between P/N: TPS2052BDGNR and TPS2052BDGNRG4?
What's G4 meaning?
Regards,
Wisan T.
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: TPS2052B Hi,
I am thinking of using the EK-TM4C1294XL microcontroller for an application, and I would like to know if there is any way to supply 5 V (800 mA) from some output of the micro.
Thanks…