Part Number: TPS2065-1 Other Parts Discussed in Thread: TPS2065 Hi team,
In the TPS2065-1 datasheet, there isn't any specification about the PowerPAD. Where it is connected.
In the datasheet for TPS2065, it said that PAD is connected to GND.
…
Part Number: TPS2065 Is it possible to obtain and share with me a copy of the TPS2065 certification body report for IEC60950-1?
Thank you.
Best Regards,
Part Number: TPS2065 Is it possible to obtain and share with the customer a copy of the TPS2065 certification body report for IEC62368-1?
Thank you.
Best Regards,
Hi Kuno,
Thank you for your reply.
First of all, I'm sorry the customer wants a TPS2052B, not TPS2051B.
Could you please confirm TPS2052B.
I think the attached document is the certification document.
Customers are looking for reports of specific test…
Other Parts Discussed in Thread: TPS2065-1 , TPS27082L , TPS2065 Hello, Could you please let me know the minnimum rise time of TPS2065-1? I can found the data of typ and max only. The customer request the 0.5ms(min), 10ms(max) of rise time when VIN=5V and 3.3V…
Part Number: TPS2065 Hello,
our customer asked about TPS2065 specification shown in below.
1) Can you tell him the specification differences between IOS and IOC_TRIP.
2) Do we understand that TPS2065 has fold back current limit topology or naturally reduced…
Part Number: TPS2065 Other Parts Discussed in Thread: TPS2066 , Hello team,
Could you tell about the latest CB test report for TPS2065 and TPS2066. Is there any update since IEC60950(Issue Date: 2016-06-20/ Report Reference # E169910-A38-CB-1)?
Thanks in…
Hi Muk-san,
Tested on TPS2065(null version). VIN connected to GND or floating; EN connected to GND.
1. Measure at point 1: Have reverse current
2. Measure at point 2: no reverse current
Same results with TPS2065CDBV.
For TI's policy, I will…
Part Number: OMAP-L138 Tool/software: Linux We are working with OMAP-L138 processor.
At custom board we use USB2.0 (USB0) interface with external clock from A3 pin (USB_REFCLKIN). During USB initialization I can't wait to get USB0PHYCLKGD bit becomes…
Other Parts Discussed in Thread: TPS2065 Hi
We have questions for TPS2065.
Do you have the answer?
1. What is the state between output pin and GND with IN:5V and EN:Low? Will it be Hi-Z?
2. What is the state between output pin and GND with IN:GND and EN…