Part Number: TPS22913 Dear supporter,
TPS22913C describe Vrcp as typical 44mV in spec.
dose TI have data how it change along with temprature within -40degC ~ 85degC?
Part Number: TPS22913 Dear supporter,
we found a problem when we use TPS22913C.
the Vin is 1.8V and Vout is 2V. Vin rise first. when EN change from low to high, Vout is 2V, seems reverse protect should trigger.
when 2V is disconnected, there shows a drop…
Part Number: TPS22913 Other Parts Discussed in Thread: TPS22976 Hi Team,
my customer use TPS22913 and TPS22976 in PE products, I want to check on next gen of those solutions.
could you please kindly share the .ppt file on roadmap of load switch in PE…
Part Number: TPS22913 Hello all, I have a question about the TPS22913B. Is the discharge transistor responsible for the output discharge always active when the ON pin is 'L'?
I would like to know, if the discharge FET is active or not when the power…
Part Number: TPS22913 Hi team,
My customer evaluates the reverse current protection of TPS22913. In Vin side there is a 3.4V supply, and in Vout side there is a 4.5V supply. When Vin=3.4V, Vout=4.5V, EN is high, will it enable the protection and how long…
Part Number: TPS22913 Hi Team,
Could you please kindly help test or do simulation on below condition? It's better if we can provide max/min value through simulation.
Cout=3.1uF, Iout=20mA, Vout=1.8V.
BRs
Given
Hello Ray,
As you have not replied in numerous weeks I will be closing this thread. If you still need help please create a new post.
Regards,
Kalin Burnside
Part Number: TPS22913 Hi Team,
just want to check if we do surge test on TPS22913 and what's the surge capacity of TPS22913.
background is that my customer found failure on TPS22913 during surge test on their products, so they want to check on it…