Part Number: TPS22929D Tool/software: Hello. I am Bumbayar I am interested in this product TPS22929D
to use it for protecting the power line and stabblize the voltage. I have two questions.
1. I want to know Vin-Vout=ΔV voltage drop and it depends…
Part Number: TPS22929D Tool/software: I cannot get a TPS22929D part to turn off, once turned on. The TPS22929D is being used as a load switch.
VIN is connected to 3.3V, with a 1uf cap at each pin.
The ON pin is being driven by a driver with 3.3V.…
Part Number: TPS22929D Hello,
we have a circuit that we want to supply from 2 different power supplies (never from both simultaneously). We have planned to use the depicted scheme.
- If power supply A is present, we supply some HW (that is not depicted…
Part Number: TPS22929D Ti Team,
Please suggest me alternate TI part for TPS22929DDBVT as this part will be available in 2022 in most online websites like element14, digikey, mouser.
Thanks & Regards,
Macjan
Part Number: TPS22929D Other Parts Discussed in Thread: TPS22860 , TPS22917 , TS5A3159-EP Hello,
I'm developing new electronics where I need to switch red high power LED and now we use this circuit:
but now I have to save space for some additional…
Hi Jani
The TPS22929D TINA-TI model has been completed and will be uploaded to the product webpage in 1-2 business days. Please let us know if you have any problems downloading it.
Thanks
Ranjani
Part Number: TPS22929D
While looking at the package on the datasheet, the package shows that the top left is Vout, but when looking at the layout recommendation shows that Vout would be in the top right. Could I get an explanation on this?
Attached…
Part Number: TPS22929D Other Parts Discussed in Thread: TPS22910A , TPS22953 Dear Specialists,
My customer is considering TPS22929D and has a question.
I would be grateful if you could advise.
---
Question
When the power is up, Vout is rising…
Hi, the device turns off when ON is connected to GND (this works without exceptions). When 5V are applied (while ON is still connected to GND) and then ON is connected to VIN it also works alright (device blocks reverse-current). Only in the described…
Hi Alek,
1. This unit was in the field for about a month. We have other units in the field as well, just haven't seen this type of issue.
2. 5.5V is coming straight from a main input regulator that gets VIn of 12V to 96V (depends on application…