Part Number: TPS2373-4EVM-758 Other Parts Discussed in Thread: UCC2897A , PMP20878 , TL431 Dear Sir 1.We plan to design a PD splitter product. but two solution (TPS2372-4 and TPS2373-4) Which one is more suitable solution.Do you have more suggestion ? Our require…
Part Number: TPS2373-4EVM-758 Hi Team,
Can I ask a question about backfeed voltage tolerance of TPS2373EVM figure 1 FET bridge?
IEEE specifies Backfeed voltage must be less than 2.8V over 100kohm. when we reuse figure-1 FET bridge configuration, can TPS2373EVM…
Part Number: TPS2373-4EVM-758
Dear Sir,
I have issue with the transistor based synchronous rectification in forward converter. When customer connects wall adapter to Target board, The reverse voltage to our board has damaged the sync fets.
how to protect…
Part Number: TPS2373-4EVM-758 Hi,
TPS2373-4EVM-758 in this EVM the capacitor location at C67(1000pF 2kV) and C5 (1000pF 2kV) were used 1812 and 1803 footprint.
Can I use same capacitor value(1000pF 2kV) in 1206 package instead of 1812 or 1803 package…
Part Number: TPS2373-4EVM-758 Can I have the specs for the transformer 750341794, because I am trying to find a replacement available on Mouser or Digikey?
Can you suggest any other replacement?
I have found these two :
1- PL300-100L (CoilCraft)
2- POE120PL…
Part Number: TPS2373 Other Parts Discussed in Thread: PMP20859
Hi Team,
My customer is surveying a POE 802.3bt Type 4 / Class 8 reference design, we found our " TPS2373-4EVM-758" should be a great solution here.
And they de have some questions…
Part Number: TPS2373-4EVM-758 Hello,
The output transient in the user guide is pretty large (~750mV/5V = ~15%), is fc just very low or is this just expected for this kind of design?
Thanks,
Michael
Part Number: TPS2373-4EVM-758 Hello,
In the EVM User Guide there is a large current spike on startup, is this real or is it some kind of measurement artifact? If real it seems like it would violate inrush requirements...
Thanks,
Michael
Part Number: TPS2373-4EVM-758 Hello,
Why are D31/D37 different parts on TPS2373-4EVM? MMSD4148T1G vs MMSD914T1G? Any reason the same part can’t be used in both places? I assume these were chosen over the BAS316 also in the design for slightly higher…