Part Number: TPS2373-4EVM-758 Dear TI,
We will contact you during the current compatibility test.
Class 5 is not recognized.
Is the calculated value correct?
Other products are class 5, 21.3 ohms.
Thank you.
Part Number: TPS2373-4EVM-758 Other Parts Discussed in Thread: PMP21318 , TL431 , UCC2897A Hi ,
My design is exactly the same as 8228.PMP21318_RevA(001)_Sch.
On my circuit board, I found that the duty cycle is not adjustable, and the duty cycle is…
Part Number: TPS2373-4EVM-758 Do we have a specification sheet for the transformer (T2) used in the design of the TPS2373-4EVM-758?
Thanks for your help with this!
Richard Elmquist
Part Number: TPS2373-4EVM-758 hello, i'm evaluating this device right now, and i'm wondering why the refernece resistor is specified as 49k9? From the datasheet it shows that the resistor will be tied to the - input of the op-amp, and the + side is tied…
Part Number: TPS2373-4EVM-758 Other Parts Discussed in Thread: PMP21318 , UCC2897A , TPS2373 Hi,
1.My design is based on 8228.PMP21318_RevA(001)_Sch,please refer to the attachment for details.
2.In the test,the voltage of vc_in is half that of VDD…
Part Number: TPS2373-4EVM-758 Hi Team.
For the C28, C68, C69, C30, C31, C32, C33 capacitor at the EVM circuit Is there a limit to the total sum capacity value?
If the sum of the capacitors is large, will not the Hot-swap circuit in the TPS2373-4 affect…
Nick,
It appears you are dead in the water.
Next time, when testing power output, just populate J15 to enable the onboard power indication LED. By shorting VDS on the primary side to the secondary side GND plane, the power converter has been damaged…
Part Number: PMP20878 Other Parts Discussed in Thread: TPS2373-4EVM-758 , TIDA-050045 Tool/software: Hi team,
Regarding the 5V/14A evaluation board TPS2373-4EVM-758, do we have reference design like PMP20878 to provide 5V/6A design?
Thanks a lot!…
Other Parts Discussed in Thread: TPS2373 , TPS2373-4EVM-758 , TPS2372-3EVM-757 , TPS2372-4EVM-006 Tool/software: We have been working on a high power POE design and have looked at all 3 eval kits for the TPS2373. Each one has a slightly different front…
Part Number: TPS2373 Other Parts Discussed in Thread: PMP20878 , PMP21318 , Tool/software: Hi , I've looked at the TPS2373-4 evaluation module and the reference designs that are provided, I want to design a PoE++ 70W PD bard that can support the PMP20878…