Part Number: TPS23753A Other Parts Discussed in Thread: TPS2372 , TPS23730 , TPS23731 , TPS2373 , TPS23734 In the design of the TPS23753A, what does the "class current requirement" refer to exactly?
Part Number: TPS23753A Other Parts Discussed in Thread: TPS23753 ,
In datasheet of TPS23753A, Vc is introduced as follows, which mentions that Cvc requires a minimum of 0.22uF, and a larger total capacitance is required to start. The design manual of TPS23753…
Part Number: TPS23753A Other Parts Discussed in Thread: PMP9175 Hi, do you have a transformer recommendation for a 5V/12.95W design (Class 3)? The EVKs and reference designs seem to only be for 7W/10W designs.
Thanks!
Emma
Part Number: TPS23753A I'm attempting to setup the APD function of the device. There are situations where I need it to run from the APD (Ethernet cable is not attached). I targeted a turn on voltage of 17V and a turn off voltage of 15V. Using the…
Hi Parag,
No problem. I will close this thread for now. Please feel free to reach out to us if you have further questions.
We wish you and your team a fantastic end to the year!
Best regards,
Diang
Part Number: TPS23753A Hi I'm Jieun,
I have a question about Power dissipation of TPS23753A
When 48V POE voltage is applied to VDD pin, how can I calculate the power dissipation?
Also, I would like to know the same, when DC 12V aux adapter voltage…
Hi Josh,
Since we have not got your response for a relative long time, I will close this thread for now. Please reply or open a new thread if you have any further questions.
Best regards,
Diang
Part Number: TPS23753A Other Parts Discussed in Thread: TL431 , TLV431 Hi Sir,
We would like to confirm the R136 is 39KΩ whether the valure is correct. because if it placed to 13.3k Ω the Voltate output is 10V rather than 5V from our design.
5228…