Other Parts Discussed in Thread: TPS24701 Hi,
Can you help me with this question?
For a high-gate-capacitance application, the datasheet of the TPS24701 says:
Gate voltage overstress and abnormally large fault current spikes can be caused by large…
Other Parts Discussed in Thread: TPS24701 , TPS24720 , TPS24700 Hello,
I would like to ask a question concerning the TPS24701.
The datasheet lists two different values of supply current when Ven = 0V.
One is given in the electrical characteristics…
Hi Furro,
Please have a look at TPS24701 Hot-Swap Controller. It is low cost and serves the purpose of Current Limiting for Startup, Over Current limit, Short Circuit protection.
You can find more information about TPS24701 here, www.ti.com/...…
Part Number: TPS24710 Other Parts Discussed in Thread: TPS24701 , Hi,
Following is the schematic of the power input circuit which uses TPS24701 as the hot swap controller.
the input voltage is 12VDC, and the max. current is about 15A-16A.
the design…
Other Parts Discussed in Thread: TPS24700 , TPS24701 Hi, I'm Byoungkil Jung from Korea.
I'm sorry because I have a poor english ability.
I have a plan to use Hot-swap controller, TPS24700 or TPS24701.
But I have some questions about this ICs.…
Hi, I found a good solution using the TPS24701. The simulation, using TINA-TI, confirms that I can achieve my goals:
- break the circuit after 5 milliseconds with DC current greater than 0.8A;
- break the circuit with AC current absoption (>100Hz…
Patrick,
TI has a number of hotswap ICs that will handle 12v/15A. The TPS24700/01, TPS24710/11, TPS24720 can do this and have EVMs build for 25A applications that are easily scaled as you need. Please see www.ti.com/hotswap for selection and design…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…
Siyu,
I think the toggle flip-flop in the block diagram on page one of the spec should have let you know that the max you will get with this device is 50% duty.
Go to page 43 and 44 of the attached and select a more suitable part.