Hi, Allen,
Sorry for late reply. I just got EVM this week, hope it's not too late. Please see the test result as below. Output voltage is not out of range from the test result.
TPS2500(no_load).txt
Device Descriptor Sweep Version Product…
Part Number: TPS2500 Hi,
We are using TPS2500 in one of our design. We are noticing a humming noise when the load is connected to USB output( Connected Pendrive). Please let us know if there a way to filter out this noise. a snap of the design is attached…
Part Number: TPS2500 Other Parts Discussed in Thread: BQ25890H , I have a TPS2500 powered from a TI BQ25890H charger. The output of that charger without a battery inserted in the system is a square wave from 3.68V to 4.2V. This results in a 400mV "ripple…
Part Number: TPS2500 Other Parts Discussed in Thread: BQ25890H ,
I have a TPS2500 regulator whose inductor (or maybe capacitor) is singing at a high frequency. It doesn't always do it, it depends on the input voltage. What I observed was when the input…
Hi,
I apologize that no one has followed up with your question. I'm going to close this thread, but if you still have a question please feel free to post a brand new thread instead of replying to this one. We will do our very best to respond within…
Other Parts Discussed in Thread: TPS2500 Can I use TPS2500 for USB OTG?? In the device mode, TPS2500 should be able to block the 5V coming from the receptacle?? How should it be implemented?
Other Parts Discussed in Thread: TPS2505 , TPS2500 We use TPS2505 Integrated USB power switch. It is not UL listed.
A similar TPS2500 is UL Listed. File No. 169910
Question - is TI planning to TPS2505 UL listed like the TPS2500. If yes, then "when"?…
Other Parts Discussed in Thread: TPS2543 , TPS2500 , TPS25200 Hi,
Can anyone help to suggest a single chip solution which supports both TPS2500 and TPS2543 features.
Thks.
Rgds,
Uma Mahesh
Other Parts Discussed in Thread: TPS2500 Hi. I'm university student in south korea. I'm not English well... sorry ;)
First, I want use TPS2500 in Orcad. but i'm not find.( i added almost libraries)
So,i ask korea TI engineer then he said "post…