Part Number: TPS2547 I want to double confirm that whether TPS2547 support 5V 2.4A. (Apple)
In the datasheet, it seems only support 5V 1A and 5V 2.1A. (Apple)
Is it right?
Part Number: TPS2547 Other Parts Discussed in Thread: TPD4S014 , TPD4S214 Hi Team,
Customer is wondering if they need to add a OVP(in case end user add a >5V source) at our TPS2547 output side, how to protect it ?
Clamping Diode or OVP part ?
Another…
Part Number: TPS2547 Hi team,
Does TPS2547 support below requirements?
- Can detect STD
- Can detect USB 1.2 STD DCP and CDp
- no USB PD
- Don't need to use I2C
Are there other recommendatons?
Best regards, Shunsuke Yamamoto
Part Number: TPS2547 Hi Team,
Customer put forward a new question about TPS2547.
At the NB S0 state, they will config CDP mode. When NB change to S3 state, they will be config SPD mode. The found the Vout will be drop. Is this normal performance? In the…
Part Number: TPS2547 Other Parts Discussed in Thread: TPS2546 , TPS2549 , TPS2544 Hi
Customer would like to evaluate 2547 to replace 2546, and from datasheet, tps2547 is drop in BOM compatible with tps2546.
Compare with spec,
1. 2547 remove sdp/cdp auto…
Part Number: TPS2547 Other Parts Discussed in Thread: TPS2557 Hi team,
I think this is a basic question.
I know some customer uses USB switch such as TPS2557 in USB host for charging USB device. Charging port controller such as TPS2547 looks like more…
Part Number: TPS2547 Other Parts Discussed in Thread: TPS2546 , , TPS2544 Hi, USB Power Switch support team
I understand that there are the difference point as the following table.
As for the feature except the above I would like know if it is backward…
Part Number: TPS2547 Other Parts Discussed in Thread: TPS2546 Hi Team,
Can someone help to double confirm that is TPS2547RTER can directly BOM 2 BOM replace TPS2546RTER ?
The only difference between them I founded was the TPS2547 has bigger continuous output…
Part Number: TPS2547
Hi,
TPS2547 is not supporting for Apple iPhone 11. We configured the TPS2547 as a CDP mode. All other manufactures its starts to charging except Apple Device.
What will be the issues, is that mode need to be changed...? Help me to…
Part Number: TPS2547 Hello, I work at a company that produces PC boards, and our client would like to have a test for the TPS2547 component, for slow and fast charge, do you have a device and sw to run this test, or is it only possible using cell phones…