Part Number: TPS25741EVM-802 Other Parts Discussed in Thread: TPS25741 I have the EVM configured for 65W with a 24v supply and connected to a device that will charge with 5v and 20v profiles only.
According to the data analyser that I am using, if the…
Hi Trevor, Please take a look at the TPS25741EVM-802 Evaluation Moduel User Guide. In section 1.1, it references the EVM's supported features of 2 output voltage selection. The TPS25741 IC itself is capable of sending USB Type C PDO of 5V,12V, and 20V…
Dear Fernandez
As below waveforms are measured from TPS25741EVM-802 for your reference,
I measured TP4(CC1), TP7(CC2) and TP16(VBUS)
1. I fixed type-c cable on the host side, only changed the SSD side, you could see the symptom is like mine, although…
Hello,
Do you currently own the TPS25741EVM? If not, I would suggest ordering that as it will give you the opportunity to work with the part and test different features from it. It can be found using the following link:
http://www.ti.com/tool/tps25741evm…
Nikhil,
The TPS25741 is designed specifically for the USB Type-C connector, using analog detection and communicating using the USB PD communication protocol to negotiate USB voltages higher than 5V.
If I understand your question correctly (trying to…
Hello,
1. Should the ISNS+- pin on the LM5175 be connected? ISNS+ and ISNS- may be either connected together or connected to ground is this function is not used.
2. What is the purpose of the smart diode on the PR2254E2? Would you recommend I include it…