Part Number: TPS25750 Tool/software: Hi,
My customer uses TPS25750 and the device only operates in sink mode(power from type-C to BQ charger). In this case, PP5V can be grounded, right? Because VBUS and VBUS_IN should be shorted together, is there any…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS65987D , , TPS25762-Q1 , TPS25751 , TPS65987 Tool/software: Hi Teams,
Our design goal:
1.Implement data conversion for Type-C interface
2.The initial idea for providing power to external…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS25751 Tool/software:
1:enable EN,sleep 850ms,read:0x22,0x03 -> get (0x04,0x50,0x54,0x43,0x48) "PTCH"
2:write 0x22,0x11,(0x06,0x80,0x3D,0x00,0x00,0x35,0x32)
3:write 0x22,0x10,(0x04…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS25751 Tool/software: I have a design based on the above components. There is an MCU writing the binary to the TPS25750 on boot. When using USB C to USB C charging, both standard USB C charging…
Part Number: TPS25750 Tool/software: If the IC has short circuit protection (overcurrent) on the PPHV line, for an output of the IC that is shorted. The datasheet mentioned VBUS to GND shorts are protected but not specifically if the PPHV bus is protected…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS25751 , BQ25731 Tool/software: Hi Experts
Client wants to save the space. Can the TPS25750D source out 5V be supported device via charger in OTG mode? this way, no need external buck 5V
Can…
Part Number: TPS25750
Dear TI,
we are currently using the TPS25750S with 2x SSM6K513NU MOSFETs for the external power path. Unfortunately the MOSFETs are not switched by the TPS.
Currently we use the TPS in dead battery mode so VIN_3V3 and PP5V…
Part Number: TPS25750 Tool/software: Hallow
I am designing a new wireless power transfer board.
We're thinking of adding some USB-PD at the output of our Rx.
Do you have am IC for 100W 5-20V USB PD ?
I prefer an "All in one" IC that includes both…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS25751 Tool/software: 1. If we are using TPS2575D as standalone PD source for smartphone charging, can the TPS2575D be used standalone in this application without using a battery or a BQ charger…
Part Number: TPS25750 Tool/software: Can you help me find the undervoltage thresholds for the TPS25750D/?
I am interested in the 9V and 15V cases.
How low can they go before we shut down?
The datasheet only mentioned an undervoltage protection on…