Part Number: TPS25921L
Hi,
We are using IC TPS25921LDR in our product. We are using this IC for overload protection purpose for communication Hub.
According to one of our test requirement, this section should not generate any radiated noise at below…
Part Number: TPS25921L Other Parts Discussed in Thread: LM66100 Hello,
My application needs all the standard circuit protection and I plan to use TPS25921L eFuse part right at the 5V power inlet into the system. Typical operating voltage and current conditions…
Other Parts Discussed in Thread: TPS25921L We have questions about TPS25921L.
Question 1.
Please tell us the time it takes from the current reaching the threshold of ILIM to shutdown.
Question 2.
Please tell us the accuracy of over-current detection…
Part Number: TPS25921L Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hello,
I am simulating the TPS25921L to protect a -15V, 500mA power supply (OUT pin connected at the PCB ground and GND pin connected to -15V output…
Part Number: TPS25921L Hello there;
I have a little problem when useing the Calculation-Sheet for the TPS25921x eFuse.
While you can set an Ambient Temperatur in the data-input table, it is not used to calaculate the
if the fuse will have a glitchfree…
Part Number: TPS25921L Hi all Would you mind if we ask TPS25921L? On our customer's circuit, FLT keeps high in spite of failure. We would like to share this information, however it contains confidential contens. So, we would like to send detail information…
Part Number: TPS25921L Other Parts Discussed in Thread: TPS25200 Hello,
Is it possible to use the TPS25921L at 50mA current limit?
Or perhaps 100mA might work in our application.
Thank you, Keith
Part Number: TPS25921L Other Parts Discussed in Thread: TPS2660 , Hi, I am considering using the 25921x or similar device as a load controller in a 13V8 (nominal) system. This question concerns the device's behaviour under EMI events and not steady-state…
Part Number: TPS25921L Hello team,
I want to know the current limit when the device is powering up with soft start.
In the beggining of powering up with SS, (Vin - Vout) is bigger than 1V. In that condition, the current limit value is not defined in the datasheet…
Hi,
I apologize that no one has followed up with your question. I'm going to close this thread, but if you still have a question please feel free to post a brand new thread instead of replying to this one. We will do our very best to respond within…