Part Number: TPS25926 Hi team,
What's the maximum OCP value of TPS259260DRCR can be set to?
Is the maximum 5.5A corresponding to 162Kohm? Rilmt can choose more than 162k? Can the OCP be set higher?
Part Number: TPS25926 Hi Team,
Could you pls check whether TPS259260 can support 12V/3.5A when the top case temperature is 80℃? Can you provide a curve of the maximum continuous current as a function of board temperature or ambient temperature? Thanks…
Part Number: TPS25926 Hi TI Teams,
Can u help to check my schematic of TPS25926?
We used TPS259261DRCR in our products, but a relatively high defect rate was found in the production testing, resulting in the breakdown and destruction as below.
Can…
Part Number: TPS25926 Hello expert,
My customer would like to check below questions. Could you kindly help to check on below questions? Thanks a lot!
Do we have max/min spec for 1A OCP (RILIM=10kohm)? Like datasheet EC table in page 5.
Do we have test…
Part Number: TPS25926 Other Parts Discussed in Thread: TPS2596 , TPS2595 Hi TI Team,
I have difficulty to tune a glitch-free startup on TPS25926 which is possible on TPS2596.
Can you help to have a look?
Can you please also confirm we can connect the…
Part Number: TPS25926 Dear Sir/Madam,
In TPS259261DRCR datasheet, it mentioned ESD human model is 2000V and charge device model is 500V. Does this means the end customer should not execute ESD test at 10KV and 12Kv test on this device, as this will destroy…
Part Number: TPS25926 Hi team, My customer did a short circuit test on the output and the device broke. TPS25926 does not reboot when I power on. Do you have any recommendations for protecting the output? Sincerely. Kengo.
Part Number: TPS25926 Hi team, I'd like to know about the current limit.
When the load current was slowly increased, the current limit was applied above the set value. Why is this? We set it at 4.3A(120kΩ), but the current limit was applied at 6A.…
Part Number: TPS25926
Hi team, Our customer would like to use the TPS25926 with USB Power Delivery. When this eFuse is back powering, the current will flow through the MOSFET body diode and to the IN pin and then to USB-C port. Is the MOSFET will turn on…