Part Number: TPS2596 Tool/software: Dear Support Team,
I tried accessing the document "11 Ways to Protect Your Power Path" by visiting the URL: https ://www.ti.com /lit /SLYY168 .
However, the link seems to be broken or unavailable.
Could you please…
Part Number: TPS2596 Other Parts Discussed in Thread: TPS2597 Hi, If my understanding of this part is correct, the shutdown of the device in short circuit failure relies on the Junction temperature exceeding the thermal shutdown temperature? This means…
Part Number: TPS2596 Hello I'd like to limit the current from IN to OUT with 0.3A limit, but also i wanna power my circuit using OUT to IN path. I possible to do that ? or is suggested to put a schottky diode from OUT to IN in order to avoid current flow…
Part Number: TPS2596
Hello team,
Can I use TPS2596 like a high side switch on the diagram below? The app note: Driving PWM Loads with TI High-Side Switches says high side switch can be used as high side protection for PWM generator (Low side Driver…
Part Number: TPS2596 Hello,
I plan to use TPS259620DDA in my design. The data sheet states that in order to select 5.7V overvoltage clamp I need to connect OVCSEL pin of the device to GND via 400K resistor. However, 400K is not a standard value. The…
Part Number: TPS2596
Hello,
I've 15V as main supply and a 12V lead acid battery to backup it.
I need a voltage limiter circuit to drive a 9~12 siren, and protect from short circuit.
TPS259621 clamp output voltage at 13.8V, using 2x diode I think…
Part Number: TPS2596 Hello,
I plan to use multiple TPS259620DDA devices in my design. These are latching parts, and my understanding is that to unlatch I need to cycle the Enable pin. So, I have 2 questions.
1. What is the minimum time to drive the…
Part Number: TPS2596 Hello, I intent to use TPS259630 to a power management equipment, responsible to supply some sensors and drivers using cables from 5 to 15 meters.
I add reverse voltage protection, and a bead on input.
I'd like to know if it…
Part Number: TPS2596
I was playing with this eFuse with an undervoltage clamp of about 2.41V and a 10.1V overvoltage clamp, I was also fusing for about .4 A using a 2k resistor as Ilm. I would like to run this system at a typical 8V but when the 8V…
Part Number: TPS2596 Other Parts Discussed in Thread: LT1054 , , TPS2661 Two quick question on Efuses.
I am building a split rail power supply for +/- 5v and +/-15 v for both 100/300 ma. I would like to use an eFuse in the design. So the question are…