Part Number: TPS2596 Other Parts Discussed in Thread: TPS25947 Hi team,
My customer is searching for E-fuse for 15V/2A and -15V/2A use case. For 15V/2A use case, I think TPS2596 is suitable. But for -15V/2A, I not sure if we have any E-fuse than can…
Part Number: TPS2596 Other Parts Discussed in Thread: TPS25924 , Hi
How can we estimate the thermal shutdown time ? In the case of configured that RLIM is 200mA, if Rdson = 150mohm, PD would be around 6mW.
If the current was inputted over the RLIM…
Part Number: TPS2596 Hello, My customer has an experience that one of our eFuse didn’t go shutdown enough fast because the board’s thermal performance was too good. At the time, they modified the board to float thermal pad to improve shutdown time.
…
Part Number: TPS2596 Hi Team,
According to Equation 12 in its datasheet, PD(Load) will be Derived as [1/6 x (Vin^2 / RL(SU)].
Could you tell the Deriving process of Equation 12?
Regards,
Takashi Onawa
Part Number: TPS2596 Hi team,
I'd like to learn about the short-circuit behavior.
The fault indication from short-circuit event may depend on the ambient temperature and use conditions, but it may take several hundred milliseconds from shorting the…
Part Number: TPS2596 Hi
Customer will use 2F for ELDC as CL and will configure that the current including inrush state does not exceed 200mA
Following the datasheet, calculating Cdvdt, Cdvdt is 420uF
As it is so large capacitance that customer…
Part Number: TPS2596 Other Parts Discussed in Thread: TPS2595 , Hello, I would like to use this part for a current limiter in an AtEx device. I need this information about the Integrated power mosfet to get the atex certification.
What I need is the…
Part Number: TPS2596 Other Parts Discussed in Thread: TPS25200 , Hi team,
customer need a ular Iq power switch in battery power supply applicaiton ,the spec as below:
Iq: 4uA
voltage limit: 3.8V ~4.2V
current limit: 80mA~125mA
small size
I…