Hi Kim,
With the maximum load current setting for TPS2596 (RILM = 453 ohms), the current limit setting typical value will be 2.004A. The minimum value of current limit for this setting can be 1.83A as highlighted below.
So,You can use TPS2596 if your…
Hi Aidan,
We are planning to release the PSpice Models for TPS2596 in the second or third week of August.
As of now, we do not have plans to release TINA models.
Part Number: TPS25961 Other Parts Discussed in Thread: TPS2596 , TPS2662 , TPS1641 Tool/software: Our customer is considering to use TPS25961.
They would like to use this when overcurrent thresholds is 120mA.
But Device ON Resistance is undefined…
Part Number: TPS25947 Other Parts Discussed in Thread: TPS25961 , TPS2596 Tool/software: Hi team,
Customer would like to know more detail about the differences of active current limit type and circuit breaker type.
1. What is the key factor to choose…
Part Number: TPS25961 Other Parts Discussed in Thread: LM5013 , , TPS2596 , TPS1641 Tool/software: Hi,
I'm currently using a TPS25961DRVR to set a current limit of 1.15A. Specification is as follows:
1.1A nominal current output. Limit must occur…
Part Number: TPS25940 Other Parts Discussed in Thread: TPS25961 , TPS2596 Tool/software: Hi,
If I wan't to use TPS25940 as Supercapacitor charger and set the charging limit for 200 mA, can I set RILMI value as 89 / 0,2 = 445 kOhm? Maximum ILIM Resistance…
Part Number: TPS25200 Other Parts Discussed in Thread: TPS2596 , TPS2597 Tool/software: Dear technical team
I'm looking for an e-fuse part similar to the TPS25200 but with current monitor capability and better (lower) Iq.
This part is for a battery…
Part Number: TPS25961 Other Parts Discussed in Thread: TPS2596 , TPS1641 E-Fuse team,
Is there a value we can select for Rlim that would allow a customer to set the current limit to 2A, and ensure it is continue to conduct at 1.8A?
Based on customer…
Part Number: TPS2595 Other Parts Discussed in Thread: TPS25961 , TPS2596 , , TPS1641 Tool/software: Hi
I'm using the TPS259533DSGT for currents as low as 100mA and the only thing I noticed was the trigger level was not within tolerance of the TPS259533…
Part Number: TPS2595 Other Parts Discussed in Thread: TPS2596 , TPS1641 , TPS25961 Dear all
I'm designing a board that has to work at 3V, 150mA max and any current over 250mA is considered a shortcircuit
On the other hand, I have to monitor the current…