Part Number: TPS25982 Hi,
・Could you please tell me about the Output voltage ramp time, TdVdt in Table 8 (Page 31)?
①Is 20ms a typical value?
If it is a typical value, could you please tell me the maximum value?
②If the values of CL and RL change…
Part Number: TPS25982 Dear TI Team:
We have Efuse-TPS25982 in our design, we checked from the datasheet which highlights "Use a Schottky diode across the output to absorb negative spikes.".
Could you share How can I check this schottky diode…
Part Number: TPS25982 Other Parts Discussed in Thread: TPS25983 Hi
Is there any efuse or hot swap available for this line that can be replaced?
for removable batteries
Do hot plug on the input
Part Number: TPS25982 HI, the question is not related to the reflow phase but on the PCB layout.
In the component datasheet you have this figure as a layout example
There is no thermal relief on the pad. Do you recommend NOT to use the thermal reliefs…
Part Number: TPS25982 Hi,
I am using part TPS259822ONRGER in a design where the input voltage is nominally 15V, whereas the device I assembled has Vovlo as 3.7V
I SHOULD HAVE used a part such as TPS25982 7 ONRGER, but only realized my mistake when testing…
Part Number: TPS25982 Hi,
We are going to use this eFuse in power side in our design with load condition. I need to know the fuse will work or not.
If the part will not work with load condition means, please recommend alternate part for our condition…
Part Number: TPS25982 Hi,
I'm testing the TPS259827O and I've configured the autoretry pins as following:
- RETRY_DLY open
- NRETRY open
As the datasheet specifies, I'm expecting the device to retry 4 times with minimum delay during an over current…