Hello Ingo,
Can you let us know the current requirement for your design?
For current up-to 0.8 A, you can consider TPS2662 device, it can pass surge test with criteria A performance.
For current up-to 6 A, you can consider TPS2663 device, it can…
Hi Yusuke-san,
Please look at TPS25200 device and Figure 18 in the datasheet for configuring the current limit threshold. This device clamps the output voltage to 5.4V till input voltage of 7.6-V, beyond that it responds as overvoltage lockout.
…
Hi Vikhyat,
TPS2660 is recommended for new designs, however if the currrent limit value is low(<800mA), then TPS2662 is recommended due to smaller size.
LM74610-Q1 is a zero Iq device (No GND pin) and is recommended for low Iq applications. However…
5140.TPS2660 Parallel Operation 02082017.pptx Hello Kazuya,
TPS2660 can be connected in parallel to increase the current limit to 4A.
Please refer to the attached document capturing the performance when TPS2660 is operated in parallel.
We have a…
Part Number: TPS2663 Other Parts Discussed in Thread: TPS2640 , , TPS1663 Dear TI Team
When operating with an input of 24V and no load, the phenomenon that the FLT pin is asserted occurs as shown in the following post. Probably the Reverse current protection…