Part Number: TPS2663-166EVM Other Parts Discussed in Thread: TPS2663 Tool/software: I am planning to use eFuse part number TPS26631PWPR in our new project, Input voltage range is 10.8 V to 52.8V, and 1.5A, Can you please provide me the reference schematic…
Hello,
Kunal Goel said: 1. Did you apply short here?
Yes
Kunal Goel said: 2. You mean VOUT went to zero first?
VOUT of PSU went to 0
Kunal Goel said: 3. Were you able to capture waveform?
No. I was not looking for the waveform, I was looking…
Part Number: TPS2663-166EVM Other Parts Discussed in Thread: TPS2663 Hi,
I plan to buy the TPS2663-166EVM to protect my devices in surge tests. The surge test level is specified as 500V/2R in this product datasheet. Does TPS2663-166EVM provide protection…
Part Number: TPS26630-33EVM Other Parts Discussed in Thread: TPS2663-166EVM Hi there,
are the schematic/layout files for the boards TPS2663-166EVM and TPS26630-33EVM available?
Kind regards,
Laura
Part Number: TPS2663-166EVM Hello team,
From the user's guide, TPS26633 is mounted instead of TPS26631 on the EVM. For TPS26631 evaluation, should we replace them by ourselves? I'd like to evaluate it with 2xILIM and non-OVP condition. If a replacement…
Part Number: TPS2663
TPS2663-166EVM devboard with TI p/n: TPS26636 soldered in. The image below shows configuration, crossed out parts are removed from the board:
VIN = 34V with high external capacitance. Vin on C4 is stable 34V during the test (not…
Part Number: TPS26630-33EVM Other Parts Discussed in Thread: TPS2663-166EVM Hi:
Is it possible to get the layout files for the TPS2663-166EVM and TPS26630-33EVM?
We are going to do a board with the TPS26632 and it would be great to see a working layout…
Hi Amrit,
We are planning to design our system to comply with the IEC 61000-4-5 surge immunity standard.
In this context, we have conducted surge testing on our evaluation board, and we would like to share the test conditions and results below…