Part Number: TPS26750 Tool/software: Hello,
The customer uses the INTEL ADL-2 platform and requires a PD chip for TPC interface connection to Type-C. The packaging requirements are smaller, with a current of 1A sufficient and no external charging. The…
Part Number: TPS26750 Tool/software: Dear TI Engineering Team,
I have two questions regarding the use of the TPS26750:
For a configuration set to operate at 48 V / 5 A, what is the typical size of the configuration file that needs to be written…
Part Number: TPS26750 Tool/software: Hi,
We are planning to use TPS26750 USB PD in our 240W sink application. We need few clarification regarding the part,
1. In sink application, whether is it required to connect PP5V pin to 5V or it can be connected…
Part Number: TPS26750 Other Parts Discussed in Thread: TPD4S480
Tool/software:
I am working with a custom design, sink only, and VBUS powered, that has a TPS26750 connected to a MCU via I2Ct, I am using a TPD4S480 as a protection chip in the configuration…
Part Number: TPS26750 Tool/software: We will use USB PD as an adjustable power supply, up to 240W, i.e. sink only.
Basically this is what we want to do.
1. Read source capability, store in MCU
2. MCU will continuously request voltage and current…
Part Number: TPS26750 Tool/software: Hi Team,
Could you please check whether we support below protocol or not?
USB PD3.2 SPR, PPS, EPR, and AVS BC1.2 DCP, UFCS, and Proprietary Protocol
Thank you,
Yishan Chen
Part Number: TPS26750 Tool/software: I'm using the TPS26750 and cannot seem to figure out the GPPI 4CC command. I've have successfully used other 4CC commands that don't require InputX data, but cannot figure out the GPPI command. I've attached an 4CC…
Part Number: TPS26750 Other Parts Discussed in Thread: TPS25751
Tool/software:
Hello, I hope you are doing well.
I’m writing this post because I have a couple of doubts regarding the EEPROM update process using the TPS with a new patch bundle. …
Part Number: TPS26750 Other Parts Discussed in Thread: TUSB211A , , TPD4S480 Tool/software: Hi team, Please review the block diagram blow, and help on the issues below:
Is it ok to use TUSB211A as signal match between TypeC1 and TypeC2.
Check that…
Part Number: TPS26750 Other Parts Discussed in Thread: BQ25756 Tool/software: Hi all,
I’m evaluating the TPS26750 + BQ25756 for a USB-C PD 3.1 source-only application to provide the full 240W (48V/5A) to a sink device. However, when using the online…