Part Number: TPS2828 Other Parts Discussed in Thread: TPS2816 , TPS2818 , Hi All,
We need to replace TPS2828 with TPS2818 or TPS2816. What would happen if we leave VDD pin of TPS2818 or TPS2816 floating. We don't have the option to tie it to Vcc unless ch…
Ultimately we resolved the problem by re-designing and eliminating the TPS2816. It was the only part exhibiting this problem (we use several other TI parts, such as uC and opamps, which all worked flawlessly) and although adding extra capacitance and…
Part Number: TPS2812 Other Parts Discussed in Thread: TPS2816 , I am using this IC to drive a MOSFET. When I check the datasheet there is a application circuit. But this circuit does not use the internal voltage regulator. I was wonder if someone can provide…
Other Parts Discussed in Thread: TPS2819 , TPS2818 , TPS2816 , TPS2817 , TL5001 , TPS2819-EP , TPS2818-EP Hello,
I was going through the datasheet of TPS28XX - EP. There was one Contradictory statement.
Statement in page 2 mentions -
"The TPS2816 and TPS2817…
Other Parts Discussed in Thread: TPS2829 , TPS2816 , UCC27517 Hi Sir,
Currently our TPS2829 test condition is Vcc = 15V, Vin = 0 V / 3.3 V,
May I know TPS2829 "positive-going-input threshold" can met our application?