Part Number: TPS3808 Hi Team,
One of my customer is using TPS3808 for their design & they have raised the queiry related to Ct calculation formula.
As per datasheet, foprmula is given as
Now as per the formula if we use 131pF in design then reset…
Part Number: TPS3808 Hi,
We are controlling the pin MR of TPS3808 with a MOSFET. But, the leak into the transistor make the MR pin to trig because of the drop into the MR pull-up resistor. This occur only when we are testing the circuit in high temperature…
Part Number: TPS3808
I wanted to clarify that these dashes really mean the production date, the top row has 4 dashes and the bottom row has 4 dashes. The top row is encrypted as the year, the bottom row is encrypted as the month of the initial week. …
Part Number: TPS3808E Other Parts Discussed in Thread: TPS3808 What is the maximum rating current ((limited current) of TPS3808 PIN6(VCC) & PIN5(SENSE)?
It was sent from the email address below.
From: myTI Product Alerts <donotreply_myti_product_alerts@ti.com>
The contents of the email are as follows.
------------Email content--------------------------
• Changes to the data sheet "TPS3808-EP Low…
Part Number: TPS3808 Hi,
According to the datasheet, the TPS3808G01DRVR is available in two package drawings. (DRV0006/DRV0006D) This is probably due to the fact that it is manufactured in more than one ASSY SITE, is there any way to tell them apart? Which…
Part Number: TPS3808-Q1 Other Parts Discussed in Thread: TPS3808 , Hi TI Expert,
Could you help to clarify the definition of the RLRESET/CLRESET in our EC table?
What does it looks like in the diagram/Schematic?
I saw same term in TPS3808 E -Q1 datasheet. …