Part Number: TPS3836 Can you tell me the maximum operating junction temperature? Only the storage temperature is given in the datasheet (150C) - does that apply to the max operating junction temperature as well?
Part Number: TPS3836 Can you suggest any alternate part number for this part number TPS3836L30MDBVREP with similar functionality which will work in ambient temperature range of -46 deg Celc to 136 deg Celc and Max Junction temperature should be greater…
Part Number: TPS3836 What is the minimum Junction temperature for part numbers TPS3836L30MDBVREP , SN74AHC1G08DBVR , SE555D ,the datasheet of these part numbers only show maximum junction temperature, so can you please provide minimum junction temperature…
Part Number: TPS3836 Other Parts Discussed in Thread: TPS3840 , TLV803E Hello,
I am using TPS3836 in my design. Unfortunately something else caused a requirement change that puts me in a difficult situation. I am comfortable with 200msec of delay (CT…
Part Number: TPS3836 We use supervisory ckt TPS3836J25DBVR. Datasheet says its ESD sensitive but does not specify level . We had it classified as a Class 1 which is typical for this type of device The parts came in specified as Class 0 which does not…
Part Number: TPS3836 Other Parts Discussed in Thread: TPS3890 , LM8365 Hello,
I'm trying to add the TPS3836 to a design. I am looking for the formula to obtain the capacitance for the timing I need.
I cannot see it in the datasheet.
Could anyone advise…
Part Number: TPS3836 Hi,
As the title, Can we connect CT pin to GND with a capacitor to modify the delay time as 20m Sec?
Or is there any method to modify the delay time?
Thank you.
That's great, thank you! Will add it for future designs. In this project I already used simple LM809; there are a couple of models for the series. With push-pull out, it looks much better when managing different inputs in multiple power ICs. Unfortunately…