Part Number: TPS40322 Tool/software: Hi,
As per the datasheet, considering the max values of HRDV & LDRV pull up & down resistances and a Rg of 5 ohms & VDD = 5V,
1. HDRV source current = 4.9/(2.5+5) = 0.65A 2. HDRV sink current = 4.9/(1.6+5) = 2…
Part Number: TPS40322 Tool/software: Hi Team,
We are planning to use TPS40322 in our design for both dual phase and single phase topologies.
Kindly find the below queries,
1. There is no support to configure or simulate a dual phase design in WEBENCH…
Part Number: TPS40322EVM-074 Is it possible to modify the output voltage of the TPS40322EVM-074 to give 2V@18A. The default setup is 1.2V@30A.
I tried using WEBENCH POWER DESIGNER but the tool always produces a single phase design.
Bill
Part Number: TPS40322 Hi,
To verify a design, I want to simulate a schematic with this part. Unfortunately there is only encrypted PSPICE model. The TINA takes ages to simulate. Can you guys send me an unencrypted PSPICE model for TPS40322? I am happy…
Part Number: TPS40322 Customer wants to control sequence through EN pin.
For TPS40322, we can pull EN to GND to disable IC, and float to enable, but we cannot pull EN to 3.3V to enable IC, right?
Part Number: TPS40322 Hi TI Expert,
A simple question about TPS40322 (Voltage Mode Control) PWM chip:
How does TPS40322 behave when the Load Current (I_dc) decreases lower than 50% of the designed Inductor Ripple Current (ΔI, or I_ripple) ? Does it…
Part Number: TPS40322 Other Parts Discussed in Thread: LM25119 Hello Team,
My customer is working with TPS40322 at voltages bigger than 5.6V (max. permitted in the datasheet). Since this is not applicable they wanted to know if we can suggest a single…
Part Number: TPS40322
Hi Experts,
What kind of master/slave mode would you recommend if we are using only one IC in a board? Master or Slave?
We encounter an issue that we can possibly fix below issue if we set IC to master mode, we thought it…