Part Number: TPS4H160-Q1 In our automotive application we are using 3 no of TPS4H160-Q1 . No. of GPIO available in systems are limited .So is there any recommendation to reduce the GPIO pins from TPS4H160-Q1?
Part Number: TPS4H160-Q1 Hello team,
TPS4H160BQPWPRQ1 can be used with 1.8V IO supply for FAULT, INx, DIAG_EN, SEL, SEH, THER signals ?
But below it shows 0-5V. Hence asked. Do you have any Electrical chara with VS=1.8V ?
Part Number: TPS4H160-Q1 I found RF noise report of TPS4H160-Q1 in E2E thread, and also I found 5MHz step RF noise in our developed PC Board. In its Functional Block Diagram of datasheet, there are two possible blocks that could be causing the noise: the…
Part Number: TPS4H160-Q1 Hi Team,
May I know the required " Solder Paste Thickness " for thermal pad of our TPS4H160BQPWPRQ1 ?
Datasheet provide the STENCIL Thickness, it's the same for Solder Paste thickness?
Thank you.
Part Number: TPS4H160-Q1 Other Parts Discussed in Thread: TPS1HTC30-Q1 , The input range of TPS4H160-Q1 is about 3.4 V to 40 V. So this high side switch is suitable to 12V system load dump. Does this HSS suitable to 24V system. If not, do we have HSS suitable…
Part Number: TPS4H160-Q1
Hi,
for tps4h160bqpwprq1 pwp0028C package, like the picture, just provide 1.2 max, can you also provide min value for customer process engineering requirement?
best regards,
jeff wang
Part Number: TPS4H160-Q1 Hi expert,
Could you pls help confirm whether the maximum current 4h160 can support can support 2.5A*4=10A current? And how to understand the several current parameters of 4h160? Thanks.
Part Number: TPS4H160-Q1 Other Parts Discussed in Thread: LM74700-Q1 Hi,
I have some question about Inductive-Load Switching-Off Clamp and Protection for Loss of Power Supply.
Q1: How does demagnetization work? The power FET is turned off slowly so the…
Part Number: TPS4H160-Q1 while Simulation using pSpice model TPS4H160-Q1, found result of leakage current is not matching with datasheet. As per datasheet it should be 3uA but we are getting only 40pA to 50 pA.
will you please help on this.
Thanks,
…
Part Number: TPS4H160-Q1 Hi team,
1.
My customer want to confirm 2 points for TPS4H160-Q1 behavior. Could you answer for this?
Please see below waveform1: CH1: IN1/3, CH2: SEH, CH3: OUT1, SEL = Low (always).
When SEL is L, the output of the OUT1(CH3)…