Part Number: TPS51200EVM Other Parts Discussed in Thread: TPS51200 , , TPS51120 , TPS51206EVM-745 Hi Team,
Posting on behalf of our customer. Does the TPS51200EVM support DDR4 applications? The TPS51200 apparently supports DDR4 but the EVM user guide does…
Hi Ni Yun,
We don't have PSRR data for TPS51200 available, however, we do have some software models available on the product page under "Design tools & simulation".
We also have an EVM that can be used for device testing located here…
Hi Katsu,
The 0.47uF is just a recommendation.
We tested TPS51200EVM with 10uF cap on REFOUT and don't see issue.
It is almost no risk to keep the existing cap on released project.
Thanks
Qian
Other Parts Discussed in Thread: TPS51200 , TPS51200EVM Hello,
I want to use TPS51200 applying power as follows.
VIN=2.5V
VLDOIN=3.3V
According to the datasheet P1 FEATURES, explain “VLDOIN Voltage Range: 1.1 V to 3.5 V”
but TPS51200EVM User…
Hi Adam,
TPS51200 is a DDR LDO controller.The thermal performance of an LDO is greatly depends on the PCB thermal pad underneath the body. I prefer the idea #2 since TPS51200EVM used two layers and 2 oz copper PCB. The EVM thermal performance looks good…