Part Number: TPS53318 Tool/software: We designed in the TPS53318 on a new board like WEBENCH created the schematic for an input voltage of 12 V and an output voltage with 3,3 V @ 4 A.
If the output is open (no load) there are 3,3 V at the output…
Part Number: TPS53318 Tool/software:
I designed the circuit using the TPS53318 chip. Could you please point out where the design is not reasonable? When the load is applied, the output becomes a pulse waveform.Please help me analyze this.
Part Number: TPS53318 Hi
I have designed a PCB for converting 16V to 5V using TPS53318 but i am not able to get the desired output.
i am getting 0.2-0.3V on the output and feedback as well.
I am adding the schematic here for your reference as i…
Part Number: TPS53318
Tool/software:
Hi,
Please verify the schematics for Vin = 12V and Vout = 1.8V.
Thanks
/cfs-file/__key/communityserver-discussions-components-files/196/TPS53318DQPR.pdf
Part Number: TPS53318 Other Parts Discussed in Thread: TPS53355 Hello!
With the same input voltage, output voltage and output current, it is not necessary to change the schematic diagram and PCB. Can tps53355 replace tps53318?
thank you!
Part Number: TPS53318 Other Parts Discussed in Thread: TPS53319EVM-136 , TPS53319 , TPS53318DQPT About the output voltage when overcurrent is detected
Modify TPS53319EVM-136 according to the attached schematic diagram.
conditions ・VIN(VREG_1P8V) 1…
Part Number: TPS53318 Other Parts Discussed in Thread: TPS53319 , Dear Team,
I would like to ask you about TPS53318 and TPS53319. 1. Are they fully pin to pin? In addition to the current capacity, one is 8A and the other is 14A, what are the main…
Part Number: TPS53318 Other Parts Discussed in Thread: TPS53319 , Hello team,
Our customer is planning to replace TPS53318 for delivery issue, and assumed if TPS53319 could be considered as an alternative. As far as I saw the datasheet, the only difference…
Part Number: TPS53318 Other Parts Discussed in Thread: TPS53353 , TPS53355 Hello team,
I would like to confirm if TPS53353DQPR or TPS53355DQPR could be considered as an alternative for TPS53318DQPR.
From the datasheet, TPS53353 and TPS53355 seems…