Part Number: TPS53513 Do we have any guidance on the distribution of soft-start time for this device (from the rise of EN)? Esp. the Max time.
We have a system that requires the device to reach regulation within 2.2msec and need to know if this device…
Part Number: TPS53513 Hi,
We are assessing the failure mode of the converter design. We would like to know if OCP threshold will change when TRIP pin is shorted to GND or floated while the converter is running.
From the datasheet I'm assuming the following…
Part Number: TPS53513 While testing start-up sequence in our design, I observed about 1ms of delay between enable and soft-start. A diagram in datasheet shows that the delay is about 400 µs. However there is also a start-up sequence waveform in datasheet…
Part Number: TPS53513 Hello.
I'm now trying to make 0.9V using TPS53513. So I have a few questions. It generates 0.9V from 12V, but 12V has switching noise of about 100kHz.
Is the only way to reduce this noise is to filter the input stage of the TPS53513…
Part Number: TPS53513 Other Parts Discussed in Thread: TPS53915 , I would like to make a design to place either the TPS53915 or the TPS53513.
Question abotu pins 27 & 28 when using the TPS53513 - if these are connected to I2C pins of a micro or FPGA and…
Part Number: TPS53513 Hi All,
A customer using TPS53513 reported an abnormal output voltage. I want to send a waveform, but I haven't got permission from the customer, so I want to share it via private message or email.
We look forward to your support…
Part Number: TPS53513 Hello,
We've been using the TPS53513 on one of our product for a couple of years without any problem but on the last batch Vout happens to be out of spec.
When the board is idle (low power), we measure FB at 0.6247 V and 0.6272…