Part Number: TPS53515 HI,
SW pin voltage is within datasheet requirement. But Vin-SW minimum voltage exceeds the SW pin requirement.
These only happen when SW is transitioning from low to high. I would like to know if these over-voltage condition cause…
Part Number: TPS53515 On p. 21 of data sheet it states that the over current protection maximum is recommended up to 14A only. Assuming the max output current including ripple current is within the saturation and heating capabilities of the output inductor…
Part Number: TPS53515 hi team,
my customer test the TPS53515 for DDR4 P2V5 rail. find the Vout will goes to higher than 2.5V. but the OVP is not functioned.
the PG the turn low, then controller make the EN low to shut down the device. do you have some…
Part Number: TPS53515 Other Parts Discussed in Thread: TPS3514 Hi
in #7.3.6 Current Sense and Overcurrent Protection
it show "For the TPS53515 device, the overcurrent protection maximum is recommended up to 14 A only. "
but in webench @ pow…
Part Number: TPS53515 Hi
in datasheet
Electrical Characteristics -->Current limit threshold, valle
RTRIP = 52.3 kΩ --> the rangy of threhold value is 10.1 - 12 -13.9 A
does anyd Influencing factors for this vaule change ?
or the value is baded…
Part Number: TPS53515 Hi
I'm Mark, QA Manager from Unigen Corp in California USA (
We are using many parts that made by TI.
Recently, we have a quality issue with TI part: TPS53515R
The defect phenomenon is NO POWER. We suspect the component have internal…
Hi Danlels,
Both TPS53515 and TPS53515A table 4, I find "device goes into forced CCM(FCCM) after PGOOD becomes high", is there an error?
Best regards,
Andy
Part Number: TPS53515 Hi,
My customer measure fsw is around 800kHz. VIn=12V, Vout=3.3V.
According to datasheet, it shows fsw spec typical value at output voltage is 3.3V.
Could you please provide fsw spec at output voltage is 5V?
Part Number: TPS53515 Hello Support team,
TPS53515 has output discharge circuit.
According to datasheet, IVODIS is defined as 10~15mA at VVO=0.5V condition.
Does it mean that discharge current depends on the output voltage condition?
Will the internal…