Part Number: TPS53632G Other Parts Discussed in Thread: UCC27512 , LMG1205 , INA170 Hi !
I am building a GaN FET based half-bridge converter with the controller TPS53632G. The parameters are:
1. Input Voltage: Vin=36-75V DC
2. Output Voltage: Vout=28V
…
Part Number: LMG5200POLEVM-10 Other Parts Discussed in Thread: TPS53632G Hi,
I am looking for the best method to program LMG5200POLEVM-10 from my computer. What USB adapter and GUI do you recommend? Is there any additional software needed to communicate…
Part Number: TPS53632G Other Parts Discussed in Thread: UCC27512 , LMG1205 , INA139 , , PMP4497 When the V5A and VDD are normal,the PWM1 and PWM2 are high level, the voltage values are about 4V, what is the reason?
Part Number: TPS53632G Hi ! I'm using TPS53632G to design a half-bridge converter. The parameters: VIN=36-75V, VO=28V, IO=10A. I 'd like to ask you a few questions about the data sheet(Revision A ) during the design process.
1、7.4.1 and 7.5.7 on the…
Part Number: TPS53632G Other Parts Discussed in Thread: TPS53632 Hi!
I have a question about using TPS53632G. If the TPS53632G is used with controlling a half-bridge conveter ,what is the max Vout of the conveter ? In addition,the TPS53632G is only used…
Hi Boris,
I apologize for the delay, but I'm still having issues getting the controller to send PWM. If you'd like to pursue the TPS53632G solution, I'll send this thread over to IPP-MPP, the product line that makes the TPS53632G controller.…
Part Number: TPS53632G Other Parts Discussed in Thread: LMG5200 , , LM5141 Hello,
I am planning to build a GaN FET based buck converter 24V to 5V @ 1A Max. Can I use any other TI’s synchronous buck controller (1MHz switching) to drive LMG5200? I don’t want…
Part Number: LMG5200 Other Parts Discussed in Thread: TPS53632G Hi Team,
A customer would like to use LMG5200 for a buck converter with the following specifications.
Input: 16-36 VDC Output: 1.1V at 10 A, 1.5V/6A, 3.3V/6A.
Do we have reference design for…