Part Number: TPS53647EVM-710 Other Parts Discussed in Thread: CSD95492QVM , TPS53647 Hi,
We need some technical help on a PoE+ related Buck converter issue. The max energy for PoE+ is 25.5W. We have a communication system that is duty cycled between transmit…
Part Number: TPS53647EVM-710 Other Parts Discussed in Thread: TPS53647 Hi,
What's the minimum and maximum output voltage of this EVM? I only see the nominal output voltage as 1volt from user guide. Can I push the output voltage to 1.8V? If not, do you…
Part Number: TPS53647EVM-710 Hello, engineer:
A total of five units were purchased, and the remaining four can be used normally. Only this one can't communicate normally。The appearance is normal and there is no damage. Use the oscilloscope to confirm…
Part Number: TPS53647EVM-710 Other Parts Discussed in Thread: TPS53647 , Please advise mechanical size of the TPS53647EVM?
Can it be used for 120A output current?
Part Number: TPS53647EVM-710 Hello, sir
I want to use TPS53647EVM-710 to do some tests. But when I lanched FUSION_DIGITAL_POWER_DESIGNER(v7.0.18), the soft can't find the device.
I'm sure that the power supply of the board is correct. And the EVM has b…
Other Parts Discussed in Thread: TPS53681 , TPS53647EVM-710 , TPS53647 Dear Sir/Madam,
Does TI have a solution similar to (TDA21472+IR35215) for 0.8V @ 200A. The following requirements. * Small size * 10mVpk-pk output ripple (max)
Regards Joe