Part Number: TPS53667 we want to know How select TP S53667 at The Fusion GUI?
The Fusion GUI will open with the rail associated with the TPS53667 controller on the [System View]
screen as shown in Figure 27 . If this were a power system that was populated…
Part Number: TPS53667 Other Parts Discussed in Thread: TPS53676 , Hello team,
I have a couple of questions to know how different TPS53667 vs TPS53676.
1) Do the both devices equip a same PMBUS control format?
2) Are the both devices have a different SMBUS…
Part Number: TPS53667 Hi Experts, I am not able to export design of DCDC converter from Webench power designer in Orcad schematic format. It is able to export in Altium format. Orcad format will be useful.
Please help. thanks, Abhijit
Part Number: TPS53667 Hi Team,
Want to check on behavior of clear_fault command.
To my understanding,it will clear all fault currently,but if the fault is still there,when reading fault register again,the fault but will be set again,right?
BRs
Given
Part Number: TPS53667 Other Parts Discussed in Thread: CSD95490Q5MC Hello,
Is any stability analysis tool such as SIMPLIS model available for TPS53667? The TPS53667 is considered with CSD95490Q5MC in two-phase configuration.
Best regards, Shinichi Y…
Part Number: TPS53667 Hello team,
In case of happening a something output fault on the one of the 6 phase outputs, is there any way to know which phase trigered the fault?
(For example, is there a register/bit to know it when the bit-0 in 0x80 frags high…
Part Number: TPS53667 Hi expert,
I check the reference circuit and always find a resistor like 10k or 121k from TSEN to GND, could I remove it?
If not, why do we add it here?
Part Number: TPS53667 Hi Team,
Just want to check on conditions to trigger rst_Vout fault.
To my understanding, if RESET pin is triggered, it will report such fault. But is there other conditions? Thanks.
BRs
Given