Part Number: TPS54060A Other Parts Discussed in Thread: LMR36506-Q1 , LMR38010 , LMR36006-Q1 Hello,
We will be using this TPS54060ADRCR IC for our project but we need below parameters:
Functional Safety FIT Rate
Failure Mode Distribution
Pin FMEA
Can…
Part Number: TPS54060A Hi team,
I can't find how we should choose the Vena value to calculate R1/R2 in equation (4) and (5) in the datasheet. Could you please clarify it?
Best regards, Iwata Etsuji
Part Number: TPS54060 Hi,
Now i have a problem about TPS54060.Before, TPS54060A is used in my DC/DC circuit.
And the circuit works properly.When i replace TPS54060A with TPS54060,and increasing load,
the output voltage drops sharply.I'd like to know the…
Hi Stephan,
The SRF1280-681 is 680uH with the windings tied in parallel. This means the nominal magnetizing inductance is 1360uH (measured across one winding with the other winding open circuit). Bourns is somewhat non-standard by quoting the paralleled…
Part Number: TPS54060A Hello, The below figure is the package mechanical data from the datasheet. I would like to know MIN and MAX values of the red underlined parameters. Are these values available?
Regards, Oba
Hello,
we use this design for several years, never had any problems and now with the latest batch we have this start-up problem.
I WANT TO KNOW WHY! The diode is a work around, not the answer to my question.
I will add this protection on future designs…
Other Parts Discussed in Thread: TPS54060A , LM46002 I have a question about TPS54060A.
Please tell us the efficiency at inverting circuit.
Vin=12V
Vout=-5V
Iout=1A
Best regards,
Takahiro Nishizawa
Part Number: TPS54060A Hi
I have questions for equation (12) and (13) from datasheet.
1. What is the parameter of Rhs?
2. How to determine parameters? (Especially, Voutsc, Fdiv)
BestRegards
Hi Frank,
Good Day. Also, our customer notices the difference in the operating temperature range on the "compare" but this information doesn't reflect on the datasheet of TPS54040, TPS54040A, TPS54060, and TPS54060A. Also, the current limit…