Part Number: TPS54140A Tool/software: WEBENCH® Design Tools Hi team,
I am using webench to design power from below specs,
Vin=10.8-28V, Vo=5V/1A, the feedback resistor is 56.2k//10k. For internal voltage reference is 0.8V, I think the resistor should…
Part Number: TPS54140A Other Parts Discussed in Thread: LMR33620 ,
Hi,
My customer requests the thermal resistance on the four-layers board condition.
Does anyone have it?
Best Regards,
Kuramochi
Part Number: TPS54140A Dear TI Team
When I carried out WEBENCH under the following conditions, the following circuit came out. Vin = 4.75-32V Vout = 3.75V Iout = 1.5A
At this time, if you check the voltage applied to the EN terminal from the voltage…
Part Number: TPS54140A Other Parts Discussed in Thread: TPS54140EVM-429 , , TPS54140 Hi
Is it enough to evaluate TPS54140A using TPS54140EVM-429?
Because there is no EVM for TPS54140A.
BestRegards
Part Number: TPS54140A Other Parts Discussed in Thread: TPS54341 Dear Forum,
My assigned customer has found some early field failures at minimum input voltage (10.8V), due to the device not starting up properly with their 60mA minimum load. As Vout…
Part Number: TPS54140A Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models I created a design with TPS54140A in webench and exported in tina-ti. I pulled-up the PWRGD pin to the output voltage (3.3V) but the simulation result…
Part Number: TPS54140A Other Parts Discussed in Thread: TPS54140 , TPS54160 , TPS54160A I have a ripple problem with TPS54140A in very small load (<50mA). The ripple wavefroms are (1) shown below. So I selected a low inductance to reduce the ripple. …
Part Number: TPS54140A Hello Can someone tell me which current I can use for formula 8 and 9. Is the inductor current IL the same as the wanted current out? If I would use formula 12 To calculate the current I need the frequency result from formula 8…
Part Number: TPS54140A Hi Robert, Thank you for your advice. Here's the lost images about preceding Q&A. This time, I use ".png" files. Because "paste a word data" couldn't be sent normally . Regards, user4778976 [Circuit] [Comparison of different inductance…
Part Number: TPS54140A Other Parts Discussed in Thread: TPS54140 The output of TPS54140A 24->5V circuit shows a large Vout ripple in case of No load.
If there exists a load resister for 20mA current , the above ripple disappears.
The follows are…