Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54260 , Hi Richard,
Customer is verifying their board with TPS54260, but there is a peak current issue of around 3A on output. Schottky diodes(NRVTSS3100ET3G, NRVBS3200NT3G, NRVBS3100T3G) are verified…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54260 Hi Team,
The customer is trying to change a Schottky diode(NRVTSS3100ET3G) to new one due to EOL. Please check the questions below and let me know.
(Vin=24V, Vout=12V, Iout=1A to 2.5A) …
Part Number: TPS54260-Q1 Hi expert,
Could you pls explain to me the principle of realizing Low Dropout(Cboot charging and discharging path)?
And If I want to design a power supply with an output of 12V, what is the lowest possible input and why?
T…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54260 Specification
Input Voltage : 9-60Vdc
Output Voltage : 5Vdc/2A
I made power supply with TPS54260. When i'm doing R&D testing without load it's working fine for full range(9-60Vdc). When…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54560-Q1 , TPS54360-Q1 Hi Sir,
My customer is looking for the pin to pin device of TPS54260-Q1 and needs to greater than Iout 3A solution.
Please let me know if you have any suggestions. Thanks…
Part Number: TPS54260-Q1 Hi Team,
My customer is currently using the TPS54260-Q1 in one of their designs and had a quick question about the minimum on time tolerance of the device. We state that this is 135ns typical in the datasheet:
Do we happen to…
Part Number: TPS54260-Q1 Hi Team,
One of my customer is using TPS54260-Q1 regulator
As per datasheet section 6.5, Is Enable threshold voltage ( min ,Max) mentioned for 25deg or for -40 to 150 deg C ?
If it is mentioned for 25 deg, could you please help…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54260 Hi,
I'm developping a board with TI TPS54260. The component is connected to a Ni-MH battery with nominal 7.2V. The battery can be discharged until 6V and the device must turn on when the…
Part Number: TPS54260-Q1 Hello,
We are using 232Kohm resistor and measuring close to 485-500KHz(from sample to sample- across 800-1000 samples) till now.
We have referred to the equation given for switching frequency calculation based on the RT but I…