Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54260 Hi Team,
May I ask how could I calculate the overcurrent value?
Here the overcurrent means when output current is higher than overcurrent, TPS54260 will shut down.
The current limit in datasheet…
Part Number: TPS54260-Q1 Hi Experts
My customer has the following questions about this device:
Section 8.2.2.1 Selecting the Switching Frequency (page 30)
“Equation 8 and Equation 9 must be used to find the maximum switching frequency for the regulator…
Part Number: TPS54260-Q1
My customer now use TPS54260-q1 but the output voltage ripple is really high.
They use to convert 12V and 24V to 5V and the yellow one is output 5V the green one is PH. Fsw=2.2MHz
We now have tried the following method but not improve…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54260 , Hello Team,
Can you explain why the different application voltages between AEC-Q version and COTS version?
http://www.ti.com/lit/ds/slvsa86d/slvsa86d.pdf
This TPS54260 non-automotive datasheet…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54240-Q1 Hi Team,
One of my customer is using TPS54260-Q1 in below configuration.
Operating Range : 6V to 18V
Normal output voltage: 5V
Normal operating current: 1.0A(Max)
Sleep or light load…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: LM76003-Q1 , TPS54260 a, Could you help to check if the TPS54260-Q1 can work normally when the INPUT: 6V and the OUTPUT:5V/<1mA.
b, when can theTPS54260 enter to PSM ,DCM and CCM
Thanks a lot
Part Number: TPS54260-Q1 Dear support member,
My customer used TPS54260-Q1. I have a question about slope compensation.
TPS54260-Q1 have function Vsen vs fsw.
Does slope compensation gradient time work advantageously differently from other current mode…
Part Number: TPS54260-Q1 Hi team.
My customer designed the power with the TPS54260-Q1
He designed 24V input and 12V output circuit.
He want to verify the circuit .
And he want to recommend capacitor capacity in compensation circuit.
I hope to share customer…
Part Number: TPS54260-Q1 Other Parts Discussed in Thread: TPS54260 Hi team.
My customer wants to design a circuit that uses a TPS54260 to output 12V at 24V input.
When Vout is shorted to GND, It must check to occur problem in automotive system.
If GND…