Part Number: TPS5430-EP Hello,
I'm currently using TPS5430DDA. However, since it is difficult to obtain, I am considering using TPS5430-EP. Looking at the TPS5430-EP data sheet, the absolute maximum rating for PH is -1.2V. The TPS5430DDA has an absolute…
Part Number: TPS5430 Other Parts Discussed in Thread: TPS5450 Hi team,
I have a question here, if I give 30V input and the output is 15V, but the current of the rear end load is only 0.01A
According to the formula for calculating the inductance,Lmin=Vout…
Part Number: TPS5430-Q1 Other Parts Discussed in Thread: TPS5450 , TPS5430 Hello,
How long will the TPS5430-Q1 be produced? Is it planned to be discontinued? I am not sure about using the TPS5430 series as the TPS5450 series will be discontinued.
Part Number: TPS5430-EP Other Parts Discussed in Thread: TPS5430 Hello,
I'm currently using TPS5430DDA. However, since it is difficult to obtain, I am considering using TPS5430-EP. Comparing the two, the TYP of Current limit is 5A, but there is a difference…
Part Number: TPS5430 Team,
A strange catch diode heating issue is observed on one of our power boards. TPS5430MDDAREP as a buck converter to step down 12V to 3.3V in one of my designs. The catch diode used is B340A-13-F as recommended in the datasheet…
Part Number: TPS5430 Other Parts Discussed in Thread: LMR33630 , LMR51430 Hi Expert,
My customer would like to know what the maximum load capacitance of TPS5430 is.
Please tdvise, thanks
Part Number: TPS5430 Hello,
Referencing slva257a and slvu243
If I configure a TPS5430 for negative output (between -3.3V and -15V), does that change the Vin range for the TPS5430.
Typically Vin is 5.5 to 36V (referenced to GND)
Does that change as GND…
Part Number: TPS5430 the sch is like this
the ph signal wave form ,those drop will cause my output ripple becames bigger,I don't know the reason.
TPS5430 is fixed frequecy 500khz,is this dc go into DCM mode?
Part Number: TPS5430 Hi team,
When tested, the chip's Pin4-tube VSENSE output test was only 0.4V, which according to the manual should normally be at 1.2V. The PIN5 pin ENA hanging VIN has been measured from DC6V-12V, and the output of VSNS has always…