Part Number: TPS54319 Tool/software:
May I ask, for this TPS54319RTER, the RC at the comp terminal usually doesn't need an additional 10nf capacitor in parallel, right? I've marked the position with an arrow.
Part Number: TPS54319 Hi,
We have a power up issue, see the image attached.
drawing attached as well
need explanation, and solution for this Fennomen.
thanks.
Part Number: TPS54319 When we use TI's DC-DC TPS54319, we often experience inexplicable burning out of this IC during use, manifested as: the input/output PIN of TPS54319 is short circuited to ground, and the root cause has not been found; Can you help…
Part Number: TPS54319 Other Parts Discussed in Thread: TPS54561 , TPS62826
Hi Ti
I wonder where the 4.6 in formula (3) from tps54319 datasheet comes from?
Because the calculation of R1 and R2 are different from tps54561 datasheet, which one is correct…
Other Parts Discussed in Thread: TPS54319 , TPS563252 Hi ,
I am looking for alternate for TPS54319 with 4.5V-17V input and 3A output current. The out voltage =3.8V
Looking Efficiency and load regulation same as that of TPS54319.
Regards
SG 1
Part Number: TPS54319 Dear Shawn Nie,
I apologize that time has passed.
My customer was checking the problem IC was placed on the evaluation board for confirmation. and communication was delayed.
I sent to your private E-mail address. I attached…
Hi Christian,
I send you email but it said "your mail box rejected my message" so I posted it here
I checked your layout and suspect the reason is caused by Vsw overshoot. For TPS54319, Cin should have very short connection to IC Vin pin(1,2) and…