Part Number: TPS54325 Other Parts Discussed in Thread: TPS54425 , TPS564257 , TPS563257 , , TPS54525 Hi team,
I want to use TPS54425 with 4.5V input and 3.3V,3.5A output.
According to the question below, the minimum duty is 78%, so 4.5V should be fine considering…
Part Number: TPS54325 Hi team
this is my customer SCH could you help me to review it ?
because I will LOA next week
can you reply this week?
there are
one TPS54325 in page1
total 1
in attached files
BRs
brian
7532.New_schematic_Power_20230309_B…
Part Number: TPS54325 Other Parts Discussed in Thread: TPS54525 , TPS54425 , TPS62130 Hi team,
My customer needs assistance.
I would like to use TPS54325, TPS54425 or TPS54525 (they are very similar) to power the FPGA core (voltage about 1V, maximum current…
Part Number: TPS54325 Hi team,
What is the min, typ, max of the rise up time for the PG signal of this device?
The only data I can see in the datasheet is this figure12 "start up"
Regards,
Ohashi
Part Number: TPS54325 Hi team,
My customer is using TPS54325 and have a question with it.
In the datasheet 8.3.2 "Power Good", it says:
" R_PG resister value ,which is connected between PG and VREG5, is required from 20 kΩ to 150 kΩ"…
Part Number: TPS54325 Hi team,
My customer is using TPS54325, which uses DCAP2 control.
For general DCDC, it is purposeful to measure the frequency responce and check the gain and phase margin to know the system stability.
But for DCAP2 control, since…
Part Number: TPS54625 Other Parts Discussed in Thread: TPS54325 , , TPS54525 , TPS54425 Hi Team,
Just want to double check, is TPS54325, TPS54425, TPS54525 and TPS54625 function equivalent and pin-compatible?
Customer is now using TPS54325 and TPS54425, but…
Part Number: TPS54325 Other Parts Discussed in Thread: TPS54425 , Hi Team,
My customer wants to know the minimum Input to Output voltage difference for TPS54325 and TPS54425, could you kindly help?
Or should customer better input the condition they want…
Part Number: TPS54325 Hi Team,
My customer wants to know Max and min range of VFB falling(fault), datasheet only have typ. value at 85%.
Do we have this data? Thanks.
Regards,
Jo