Part Number: TPS54360B Other Parts Discussed in Thread: TPS54360 Hello,
When downloading the TPS54360 average model off of ti.com and running, we get the error below. No changes were made, just opening and running. We have replicated this error on two different…
Part Number: TPS54360B Other Parts Discussed in Thread: TPS54360 If we design a TPS54360B for 2.1A , 3.1Vload at peak, how can I make sure the buck will be stable if the load transience is at 10Khz from max to min on the load side.
Also the input voltage…
Part Number: TPS54360B Other Parts Discussed in Thread: TPS54361 , TPS54360 , LM76003 hello TI engineers
I would like to use TPS54360B for make a negative voltage of -15V, with input voltage 24V.
I would like to use TPS54360B as in a buck-boost converter…
Part Number: TPS54360B Other Parts Discussed in Thread: TPS54360 Hi,
I have a customer used the TPS54360BDDA having a problem. He reported that occasionally there would be buring phenomenon,but the cause has not been identified.
So I would like to ask…
Part Number: TPS54360B Other Parts Discussed in Thread: TPS54360 Hi Team,
My setup, Vin->TPS54360B->Battery Charger | Load | LDO
Functionality:
Q8 is OFF when Vin is ON and TPS5360B is giving an output.
Q8 is ON when there is no output form TPS54360B…
Part Number: TPS54360B Hi,
I have used this ic for one of my product?
Can you please how we can shutdown the IC voltage goes beyond maximum limits i.e 65VDC
I need to implement same logic for our circuitry to avoid any over voltage issues during operational…
Part Number: TPS54360B Other Parts Discussed in Thread: LM5088 , Hi Team,
I intend to use the reference design mentioned in the document (1) SNVA681A – March 2015, page no. 5
Figure 6. Load Dump Protection Application Circuit, attached the image for…
Hello,
Do you measure large SW node overshoot when operating at 42V? I realize that the input capacitors are rated for 50V and you are testing at 36V to 42V. At this voltage level the effective input capacitance will be significantly lower than the rated…
Part Number: TPS54360B-Q1 Hi team,
Our customer, Mitsubishi, requests us to review the schematics of TPS54360B-Q1.
Could you support this request?
The input capacitor is very small, but is there others points to be needed modification in customer schematics…
Part Number: TPS54360B Hi Team,
My customer plans to do short-circuit test on TPS54360B, and I am wondering the short-circuit protection scheme of TPS54360B.
According to the datasheet, the frequency foldback scheme can help inductor current to ramp down…