Hi Akashi:
see TPS54429 result, I also attached modified simulation files, pls try it. you may need take care of the load resistor to make sure it is not over loaded
slvm375_TPS54429.TSC
thanks
Part Number: TPS54429 Dear team,
Could you help to confirm VIH of EN pin?
In device datasheet, the minimum of VIH is 2V. But we test on our board, device is enable once EN voltage level higher than 0.77V.
And I find an E2E post, the EN threshold is around…
Part Number: TPS54429 Dear team,
I check with datasheet and there are no latch protection for TPS54429.
We do power on/off cycle testing for TPS54429, but output voltage does not present even Vin back to12V. We have to remove input power and wait input…
Part Number: TPS54425 Other Parts Discussed in Thread: TPS54429 , Hello teams
We want to check the behavior of TPS54429/TPS54425 with 12vin/5vout setting on TINA TI. But it's output ramp up only til 4V on our design. And Both Vout level is decreasing…
Part Number: TPS54429 Hi,
I would like to ask you about the TPS54429 device. The formula for calculating the frequency Fp with L1 and C8 + C9 of Output Filter Selection is described in the data sheet. Please tell me how to think about the design target…
Part Number: TPS54429 Other Parts Discussed in Thread: TPS54225
Hi sir,
Did you create a DFMEA report for this part?
you can sent it to me by email if you have it.
Thank u so much.
Regards,
M
X1054259@TI.com
Part Number: EVMK2GX Other Parts Discussed in Thread: LP2996A , TPS65911 , TPS54429 , In the schematic EVMK2GX, what's the purpose of TLV707085DQNT, TPS54429 and LP2996A respectively in the schematic? ( Regulators other than TPS65911)
Could you tell me…
Part Number: TPS54429 Hi
because the MOSFET are in the converter, the spec only show the SW(low side MOSFET) max voltage=22V.
We want to know the high side MOSFET max voltage=?
Thank you!
Part Number: TPS54429 Dear E2E,
could you please help to provide bode plot of tps54429 at 12Vin, 1Vout/4A?
Similar condition is also ok.
we just want to get a reference one to compare what we measured and also to see what it looks like.
BR,
Jason