Part Number: TPS54561-Q1 All simulations for a power supply I was redesigning failed. I tried to redo a simulation on one of my previous designs (without any change) and it failed too. I believe the server running the simulations is down.
Part Number: TPS54561 Hi TI
I want to know that TPS54561 Oscillator type is a voltage controlled oscillator or not? Like ADI LTC3707 which supports switching frequency selection continously by PLLFLTR PIN voltage . thanks.
Part Number: TPS54561 Hi team:
My customer want to use TPS54561 at this parameter, wanna to check how make this 100% can work, and got confuse use some cal-tool for reference. Can you help to take a look?
tks!
Vin 24v
Voutput 23V 3A, 500khz. …
Part Number: TPS54561-Q1 Other Parts Discussed in Thread: TPS54160 , , TPS54561 Hi,
Can you please provide the tool regarding the compensation network.
See the below image for reference from MPN - TPS54160. I want the same tool for MPN - TPS54561…
Part Number: TPS54561 Hi all,
i used a TPS54561 in my desing with following parameters:
Input Voltage 48V, Output Voltage 13.8V Output current 5A, Switching frequency 600kHz.
The converter works fine, until i reach a 2.5A at the output. Then the…
Part Number: TPS54561 Hi TI
For the Figure 8-1. 5-V Output TPS54561 Design Example of TPS54561 datasheet Rev.G,
Start input voltage (rising VIN) = 6.5V
Stop input voltage (falling VIN) = 5V
Then, we get Ruvlo1=441k and Ruvlo2=90.9k by equation…
Part Number: TPS54561 Hi TI
From datasheet TPS54561 Rev.G
7.3.4 Low Dropout Operation and Bootstrap Voltage (BOOT): The recommended value of the BOOT capacitor is 0.1 μF.
8.2.1.2.8 Bootstrap Capacitor Selection: A 0.1-μF ceramic capacitor must be…
Part Number: TPS54561 Other Parts Discussed in Thread: TPS54560 , TPS54560B Dear team
The customer would like to know, what is the difference between TPS54560 and TPS54561?
Could you help to recommend?
Many thanks
Denny
Part Number: TPS54561 Other Parts Discussed in Thread: TPS7A94 , TPS717 Hi,
We are using TPS54561 with LDO,It is for LNA bias supply. Is an additional filter required to meet the CISPER32 standard at the output and input of TPS54561?
*TPS54561 output…