Hi Fujiwara-san,
We haven't heard back from you, so we're closing this thread. If you've resolved the issue, kindly click "this resolved my issue" or let us know how it was fixed so that others who face similar issues can benefit from your experience.…
Part Number: TPS546D24AEVM I understand the process of converting TPS546D24AEVM from 2 phase to single phase.
What changes has to be made to the output decoupling capacitors and the compensation circuitry with respect to 1 phase vs 2phase.
Part Number: TPS546D24A Hi
I have connected the external load with TPS546D24AEVM (single phase) and monitored the current consumptions on the TI fusion tool with different loads (1A,2A,3A,4A,5A, and 6A). The current showing on the tool is not a match…
Gajendiran A said: We are probed using Tip and Barrel parallel to the capacitor.
The probe is not calibrated, and the amplitude exceeds the margin. After adjusting this, the probe compensation. Now, the ripple voltage is 60mV.
It's good to see that the…
Part Number: TPS546D24AEVM Hi,
I'm trying to download the " FUSION_DIGITAL_POWER_DESIGNER " software but the link is not working.
Regards,
Gajendiran A
Part Number: TPS546D24AEVM Hello
How to output 80A at 0.5V using TPS546D24AEVM-2PH?
Could you provide config file for output 80A at 0.5V?
Best regards.
Part Number: TPS546D24AEVM Other Parts Discussed in Thread: TPS546B24A , TPS546A24A Dear TI,
Here are some questions I came up with while working with the TPS546D24AEVM. Thank you for answering.
The default value for VIN_OV_FAULT_LIMIT is 0015 (verbatim…
Part Number: TPS546D24A You have an eval board titled: TPS546D24AEVM-2PH which I purchased online.
How can I get the source codes for this design?
Please provide the link of the source codes of this EVM:
Regards,
Abdus
Part Number: TPS546D24AEVM Other Parts Discussed in Thread: TPS546D24A , TPS546D24 I'm using the TPS546D24AEVM-2PH to test configurations before programming actual boards. I am running into some problems:
The power controller is reporting an IOUT of…