Part Number: TPS548A20 Hello,
My team and I are working on a thermal analysis for our design using ANSYS ICEPAK and I am having a hard time finding thermal models TPS548A20. Currently we are using the thermal resistance values of the ICs from the datasheet…
Part Number: TPS548A20 Hello,
My customer had an issue as the link below on the TPS548A20 they designed.
- https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1230796/tps548a20-device-failure-history/4651108
Recently…
We've been searching for the route cause like the below.
1. +12VIN-EPAD / +12VIN-PGND almost shorten (ohm analysis in the picture) in TPS548A20(which is 3.3V source) in case #1 Board.
2. IN that board : CPU uses its power source from 1.05V and 3.3V…
Part Number: TPS548A20 Hi Team:
Customer use TPS548A20 for low noise RF case, can you help to review attach SCH and layout?
tks advance.
TPS548A20-4 Y1.zip
Part Number: TPS548A20 Hi team:
can you help to send the IBIS model for TPS548A20 device to me? My customer want it for PI and SI simulation。
tks for your checking.
Part Number: TPS548A20 Question 1: Output Capacitance Range:
The datasheet indicates that we should try to set the 2-pole L-C filter at a frequency at or below the internal zero frequency (between 6 and 12kHz). This approach results in an unrealistically…
Part Number: TPS548A20 Hi,
We are using TPS548A20 to generate 1.0V @ 10A from 12V.
1.0V goes to Load(MPU) from regulator,
Vout trace which connects feedback resistors(Rtop,Rbot) is coming from Load side in Internal Power plane. This power plane has one…
Part Number: TPS548A20 Hi,
On the page #6 of TPS548A20 data sheet, i saw "PGOOD in from higher", "Delay for PGOOD going in",
can you tell me what " PGOOD in" and "Delay for PGOOD going in" means?
Thanks,
Tony