Part Number: TPS548B22 Hi,
1. As shown in the following two pictures, the output voltage of BP LDO is written as 2.9V in one place and 5.07 in the other place. Why is it different?
2. What do the following two tables describe?
Part Number: TPS548B22 Dear team,
Could you help to check why device have a ring when output voltage close our design target?
Attachments are waveform and schematic for your reference. Thanks.
Regards,
Ben
Part Number: TPS549B22 Other Parts Discussed in Thread: TPS548B22 Hi Expert,
I use the TPS548B22 and we face a shortage of that part, Can i directly use the TPS549b22 as a 2nd source? Thanks.
I check the datasheet, i found 2 difference.
1. pin1,2,3 will…
Part Number: TPS548B22 Hi Experts,
Seeking your assistance on this query:
Can AVS (adaptive voltage scaling) be implemented with TPS548B22? The load device requires 0.8V with +/-0.2V. The load has an output that can be used in a feedback loop of the voltage…
Part Number: TPS548B22 Other Parts Discussed in Thread: TPS548D22 , Hi Team,
When replacing TPS548B22RVF on an existing design with TPS548D22, the 40 amps device, 2 sw pins and 2 vin pins are not connected.
Is this a problem when only using it as it is…
Part Number: TPS548B22 Other Parts Discussed in Thread: TPS548A20 , , TPS544B20 Hi team,
Customer is doing a 5V input switch project, and they want to check with us if TPS548A20 TPS548B22 TPS544B20 could support 5V input and 3.3V output application, datasheet…
Part Number: TPS548B22 Other Parts Discussed in Thread: TPS53353 , Hi Expert,
We are proposing the TPS548B22 to replace the TPS53353 for better supply.
But the end customer defined the 15k~300khz range for unity-gain bandwidth need to met for AVS control…
Part Number: TPS548B22 Hi team,
My customer is using our TPS548B22 and the schematic is as below.
I have checked it and would like to have your double confirm.
Would you have any suggestion about it? Thanks.
Part Number: TPS548B22 Hello Admin,
I have a question about using TPS548B22 for Xilinx FPGA.
0. Web bench setting is like the below.
- Input: 12-14V
- Output: 0.87V
- Output current: 25A
1. Out circuit diagram is different from Web bench output and…