Part Number: TPS55288 Tool/software: Hi team,
Customer wants to use TPS55288-Q1 for non-auto application due to some reason.
Could you please list all differences?
Best regards,
Hayashi
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: TPS26743E-Q1 , USB2ANY , TPS55288 Tool/software: Hi,
Can I talk with the TPS55288-Q1 via I2C without an input at Vin? The datasheet for the part and the evaluation board show that an external…
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: TPS55288 , TPS552882 , TPS61299 Tool/software: Hello, We are going to use TPS55288-Q1 for 3.3V and 5V regulators from an input power supply between 2.8V and 5V, our Questions are: 1- Is TPS55288…
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: TPS55288 , TLV61048 Tool/software: Hi guys,
I've recently got to know the DC-DC TPS55288 buck-boost series which in theory is perfect for my application.
However, I'm struggling with it and…
Part Number: TPS55288-Q1 Hello Expert,
Our customer is considering to use 1KHz FMOD DITHER function for EMI issue.
Then, they'd like to understand pros/cons of this.
As far as I confirmed, biggest cons is output voltage variation. Also, I found…
Part Number: TPS55288-Q1 Tool/software: Dear TI team,
I would like to inquire whether the TPS55288-Q1 can meet the requirements of output voltage: 5~12V and operating current: 7A. If not, are there any similar ICs that can satisfy these conditions?
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: TPS55288 Tool/software: I would like to use this converter for a stand-alone application, so I need to know if the I2C connection in mandatory or the HW configuration pins are enough to its correct…
Part Number: TPS55288-Q1 Tool/software: All:
Is there a way to simulate fault conditions without actually generating?
For instance, I do not want to create a short circuit on the device, but I would like to be able to set a bit in a register that…
Part Number: TPS55288-Q1 Hi,
May I know what is the different for TPS55288QRPMRQ1/TPS55288QWRPMRQ1?
I found the package information all the same. thanks!
Thanks!
Jeff
Part Number: TPS55288-Q1 Other Parts Discussed in Thread: TPS55288 Glad to see you,
I'm considering setting up a WCCA simulation environment using the Spice model of TPS55288-Q1 supported by TI website.
First of all, I'm checking whether the temperature…