Part Number: TPS55289
Hi Expert,
I find some difference between TPS55289-Q1 datasheet and real test wave about I2C communication. Below is the photo. When I set the delay time between "ack" and "DATA" as datasheet time sequence, the communication…
Part Number: TPS55289Q1EVM Other Parts Discussed in Thread: USB2ANY , TPS55289 , TPS55288 Tool/software: The GUI can connect with the USB2ANY , but can't connect with the EVM through I2C whatever the addr is 74H or 75H , the TPS55288EVM-530 has the same…
Hi Murali,
For TPS55289, the output voltage can only be enabled after writing 1 to internal OE bit. So without I2C, TPS55289 can't output the target voltage.
And we are going to release TPS55289-Q1 which is optional to output 5V default voltage. You…
Hi Christian,
Sorry for late reply.
1. From my calculation, for 400kHz switching frequency, 36Vin to 1.5Vo is a critical boundary because of min Ton, you can also decrease the switching frequency to get a lower duty cycle.
2. TPS55289 is a full…
Part Number: TPS55189-Q1 Other Parts Discussed in Thread: TPS551892-Q1 , TPS55289 Tool/software: Hi All,
I have a question about the TPS55189-Q1.
Which is effective: setting the EN pin high, or setting the MODE Register (Address = 6h) to 0b (output…
Part Number: TPS551892-Q1 Other Parts Discussed in Thread: TPS55289 , TPS552892 Tool/software: Hello,
I see that TPS551892-Q1 is now yet in Webench as of yet. Can you provide any design examples to aid calculating critical component values?
Thanks…
Part Number: TPS61088-Q1 Other Parts Discussed in Thread: TPS61088 , TPS55288 , TPS55289 Tool/software: Hello,
Anyone knows how to fix the VCC output at 5V? The datasheet is not clear but seems to imply that the output voltage is around 5V but Vin dependent…
Part Number: TUSB4020BI-Q1 Other Parts Discussed in Thread: TPS55289 , TPS25772-Q1 , Hi Team,
Project: Automotive PD USB Charger&Hub:
With 2 ports for output, one is a charge only port and another one is a charge + communication port.
The overall…
Hi Max,
To confirm, TPS551892-Q1 can be used as constant current source for super cap charging. It is a simple solution without rich features. To discuss, I am wondering why do you choose this part instead of a BQ part? Sorry for confusing you.
About…
Part Number: TPS552892-Q1 Other Parts Discussed in Thread: TPS552892 , TPS55289 Tool/software: Hi, Ti Engineer.
I'm reviewing to apply TPS552892 as below. One question is that in datasheet, it is recommended to set a frequency below 500 kHz due to power…