Part Number: TPS552892-Q1 Tool/software: Hi team,
Could you help check if 552892 could support below condition?
VIN_min=5.6V Vout=6V Iout=6.5A
Best regards
Fanbin
Part Number: TPS552892-Q1 Other Parts Discussed in Thread: TPS552882-Q1 Tool/software: Hi team,
Can you please help review my customer Valeo TPS552892-Q1 design as below? Thanks
TI_BUCK-BOOST_TPS552892QWRYQRQ1_review_file_20250327.pdf
Best Regards…
Part Number: TPS552892-Q1 Other Parts Discussed in Thread: TPS55289-Q1 Tool/software: Hi,
Our project is using TPS552892-Q1. We set RSNS to 10mΩ and VOUT to 12V as shown below. So the current limit should be 5A.
Step1:TPS552892-Q1 is enabled and…
Part Number: TPS552892-Q1 Other Parts Discussed in Thread: TPS63070 , LM51772 , TPS552892 Tool/software: Hi, Brice, How did you determine the -2.5A? how much can it source?
Hi Janos, Andrew,
Thanks for the discussion, TPS552892 can be used as…
Part Number: TPS552892-Q1 HI
would you be able to offer any recommended heatsink solutions for the (TPS552892QWRYQRQ1) DC-DC converter VQFN package, this is a small size of 5mm x 3mm but it could need to dissipate 30 watts or so. Thanks
Regards…
Part Number: TPS552892-Q1 Tool/software: Hi Expert,
Have a good day.
I have one question about the mode change between BUCK and BOOST.
In DS: When the input voltage is close to the output voltage, the TPS552892-Q1 operates in one-cycle buck and…
Part Number: TPS552892-Q1 Tool/software: Dear team,
My customer would like to use TPS552892-Q1 for their application.
- Input 9V~16V / outtput 12V_4A
but there is question regarding EN/UVLO operating condition.
At datasheet, we can see Absolute…
Hi Jackson,
Thank you for reaching out. Below is my comments.
1. Recommend to add one E-CAP in input side to stabilize input voltage.
2. Recommend to use >16 rated voltage cap for C3 to ensure 2uF effective capacitance with 5V DC bias.
Jackson…
Part Number: TPS552892-Q1 Other Parts Discussed in Thread: TPS552892 , LM2611 , LM5157 , , LM63635-Q1 Hello,
I am looking for a schematic - using the TPS552892- converting positive voltage (12V) to a Negative Voltage (-15V) .
Regards,
Giora
.
Part Number: TPS552892-Q1 Other Parts Discussed in Thread: TPS552892 Hi Team
below is customer application for TPS552892. do you think the capacitor is proper? they spec for all power rail is 50mV.
Vin
Iin_max
Vout
…