Part Number: TPS562200 Hello,
We need help here to solve RE testing failure issue.
We are doing RE test in one of the project and we are facing RE failure issue since long time and we have tried multiple iterations to solve it but still we do not have…
Part Number: TPS562200 Dear TI:
一、In TPS562200DDCR datasheet Recommended Operating Conditions,as shown in the left figure,There are two parameters for Operating temperature:TJ:-40 to 150℃ and Recommended Operating free-air temperature is -40 to 85℃.So ,Is …
Part Number: TPS562200 Hello everyone,
I want to convert 12V to 5V using the TPS562200.
I have attached the schematic via the link below.
I initiate the simulation with a Stop Time of 10ms in Transient, but I encounter the error provided in the link…
Part Number: TPS562200 Regarding the parameter calculation of Snubber circuit, I have the following questions, please help to point out:
The first question: I have seen different descriptions of Rsnb values in different application manuals of TI. Would…
Part Number: TPS562200 Other Parts Discussed in Thread: TPS563200 , Hi,
I'm reaching out to see if TPS563200 is compatible to be a direct replacement for the TPS562200. Are there any potential issues one should be aware of when using these devices interchangeably…
Part Number: TPS562200 Hi,
I'm reaching out to find what the behavior of VOUT is when the EN pin is disabled. I assume it would result in no voltage on the output in this scenario. If you have more information about the expected VOUT behavior please…
Part Number: TPS562200 Hi Team,
My customer is working with TPS562200.
They are wondering Why the output voltage range only reach 7V.
They circuit original Vout is 8V.
Can they design 8V too?
What's the problem if exceeds the recommended output voltage…
Hi Jafar,
Got it. It's suggested to share more waveforms for me to debug, especially the issue waveform. or is it ok to have a meeting to discuss? Based on current waveforms, the information is small. It's difficult to find the root cause.
BRs…
Part Number: TPS562200 Problem is a reoccurring failure with the TPS562200 when implemented as per the attached circuit diagram. Typically there are two scenarios, first is the EN pin stops functioning leaving the device always on, secondly the device…
Part Number: TPS562200 Hi,
I have used TPS562200ddcr to convert my 12VDC to 3.3VDC.
While testing the module on my PCB I noticed that I receive the appropriate 3.3V output as desired but the output current seems to be oscillating and reaching a negative…